GARANT

GARANT history:

Today is tomorrow's yesterday.

Nothing is more constant than change. 1973 marks the start and at the same time the origin of the GARANT brand in the area of machining. Since then, GARANT has made continual developments on your behalf so that, even the day after tomorrow, you will be at the head of the pack with the innovative premium quality from GARANT. The GARANT story – discover selected innovations and highlights:
  • garant1973.png

    1973

    GARANT Brand

    The GARANT brand is launched as the "clever alternative" in the field of machining.

  • garant1981.png

    1981

    Development start-up

    Start of development of the GARANT milling cutter range

  • garant1983.png

    1983

    GARANT milling cutter range

    The new GARANT milling cutter range is officially launched

  • garant1990.png

    1990

    End mill world premier

    Introduction of the world's first end mill as a 3-fluted version with 45° helix angles

  • garant1992.png

    1992

    GARANT Softcut

    Introduction of the new geometry for a reduction of cutting force

  • garant1994.png

    1994

    ISO 9001 certification

    We are the first sales company in this sector to be certified like a manufacturer

  • garant1998.png

    1998

    GARANT spanners and sockets

    Complete range of heavy-duty GARANT spanners and sockets launched onto the market

  • garant1999.jpg

    1999

    Research project

    GARANT achieves top results in the Kassel University research project "thread cutting in magnesium"

  • garant2001_1.png

    2001

    VDA 6.4 certification

    Further certification by the German Association of the Automotive Industry (VDA) underscores our manufacturer competence

  • garant2001_2.png

    2001

    GARANT machining handbook

    The first compendium of the industry, comprising more than 500 pages

  • garant2002.png

    2002

    GARANT colour coding system

    We are the first in the industry to introduce a system of colour coding for consistent machining of components

  • garant2003_1.jpg

    2003

    GARANT celebrates 30 years

    Release of the GARANT "anniversary box", containing a unique range of products, to mark
    the brand’s 30th year of existence

  • garant2003_2.png

    2003

    GARANT Diabolo

    The new type of coating developed especially for the hardest materials makes the GARANT Diabolo milling cutter range an immediate success

  • garant2004_1.png

    2004

    German market leadership

    With GARANT we become Germany's market leader in the field of solid carbide drilling and milling

  • garant2004_2.jpg

    2004

    Campaign

    The GARANT "animals" campaign is launched and receives numerous prizes and awards

  • garant2005.png

    2005

    GARANT powercard system launch

    The first "fully comprehensive insurance" for GARANT power tools, in a handy credit card format

  • garant2006.png

    2006

    GARANT MM1

    Introduction of the MM1 measuring microscope, a new HPC milling cutter range with ZOX coating, and the ToolCar

  • garant2007.png

    2007

    iF Award

    The GARANT torque wrench is recognised with the iF Award; in addition, the MTC milling cutter range is launched onto the market

  • garant2008.png

    2008

    GARANT Zeroclamp

    Introduction of the innovative zeropoint clamping system

  • garant2010_1.png

    2010

    GARANT 360°Tooling

    The premiere of the first all-round service for more productive machining processes

  • garant2010_2.png

    2010

    Modern materials

    Innovative cutting tools for new types of material open up new market segments for GARANT

  • garant2011.png

    2011

    GARANT ECO

    With "efficient cooling" GARANT sets new standards – just as with TopCut and the tooling range for lightweight components

  • garant2012Tieflochbohren.jpg

    2012

    GARANT deep hole drilling

  • garant2013HiPerDrill.jpg

    2013

    GARANT HiPer Drill