Click&Clamp with double clamping
31. mar. 2020
But this is not all. The Hoffmann Group has also expanded the GARANT Xtric range by four new base lengths. For the first time, the GARANT Xtric is also available in size XS with a base length of just 136 millimetres for processing small components. This means sizes XS, S and M are now available in a jaw width of 80 millimetres. In addition to this there are new vices with a jaw width of 125 millimetres, 32 kN clamping force and a length of up to 270 millimetres in the sizes XS, S and M. All models are alternatively available with pivot jaws. This means the customer can choose between six vice sizes, which are each available in two variants.
The GARANT Xtric can be converted into a double vice quickly and easily: the user simply has to change the standard spindle bearing and insert the centre jaw. The jaws, which can be rotated 180 degrees and interchanged precisely to the micrometre, are then put back in place. Thanks to the click mechanism, this is performed in no time at all, and with GARANT gripper jaws, blanks can be clamped without pre-stamping. Top jaws suitable for the “LANG” system are also available. All models are equipped with an endutec automation interface, which can be used as a coolant hole, as well as gripper mounting holes on both sides as standard. This makes them suited to a wide range of automation strategies.
In addition, the GARANT Xtric offers the following for attachment to the machine table: longitudinal slots, holes for the “LANG” positioning system with a pitch of 52 or 96 millimetres, as well as adapter plates for clamping on the GARANT Zero Clamp zero point system or other zero point clamping systems.
The new centring vices can be ordered with immediate effect and can be delivered from 1 April 2020.