Hoffmann Group Home
  • 500.000 listed articles
  • Highest delivery accuracy
  • TÜV certified quality of delivery
  • Menu

Press Releases

10 May, 2019

Hoffmann SE appoints spokesman for the Executive Board

Europe’s leading system partner for quality tools appoints Martin Reichenecker as spokesman for the Executive Board with immediate effect. Mr. Reichenecker will remain Chief Sales & Marketing Officer (CSO).

GO TO PRESS RELEASE

Reichenecker-400x800.jpg
-
18 Sep, 2018

Full speed ahead – with GARANT Power Q

Milling with very high feed rates, without compromising process reliability – this is why the Hoffmann Group has now brought the new GARANT Power Q product family on to the market.

GO TO PRESS RELEASE

GARANT Power Q 400x800.jpg
GARANT Power Q indexable inserts are available in three system sizes, for steel, hardened steel, stainless steel and titanium.
17 Aug, 2016

Hoffmann Group opens first subsidiary in the United States

The Hoffmann Group, Europe's leading system partner for quality tools, has officially opened its first subsidiary in the United States.

GO TO PRESS RELEASE

IMG_6103_kleiner.jpg
-
30 Jun, 2016

GARANT MasterSteel opens up a new performance class for solid carbide drills

The Hoffmann Group, Europe's leading system partner for quality tools, has expanded its GARANT MasterSteel product range with two new solid carbide drills, thereby further extending its lead over the competition when it comes to machining technology.

GO TO PRESS RELEASE

MasterSteel SPEED and FEED_400x200.jpg
-
24 Jun, 2016

New platform for sharing information and expertise now on air

The Hoffmann Group has launched the Hoffmann Group TV online channel as an outlet for its film content. Through this new video portal, Europe's leading system partner for quality tools is now offering its customers a quick, convenient way of obtaining information on professional machining, milling, drilling, turning, measuring and grinding as well as state-of-the-art workstations and storage solutions – all from a single platform.

GO TO PRESS RELEASE

Hoffmann Group TV.jpg
-
21 Jun, 2016

GARANT HB 7010-1 turning grade: the highest cutting speed for maximum productivity

The Hoffmann Group, Europe's leading system partner for quality tools, is introducing a new turning grade for steel machining to the market. The new GARANT HB 7010-1 turning grade was developed to achieve wear resistance at the highest cutting speeds.

GO TO PRESS RELEASE

LP-HB7010-1-800x400.jpg
-
8 Mar, 2016

LogiMAT 2016: GARANT access technology now with Easyfix hooks and holders

The Hoffmann Group is set to launch its new access technology products for the first time at LogiMAT 2016, in hall 5, stand 5D55. The new GARANT aluminium stepladders impress with added ergonomics and safety. This is ensured by the new Easyfix hooks and holders, which can be fitted simply to the side rails without the use of tools, making it easier and safer to carry electrical equipment and tools. This means that important equipment is always quickly to hand. As a result, working becomes more comfortable, more efficient and safer.

GO TO PRESS RELEASE

GARANT-Leitern-800x400_neu.jpg
GARANT access technology now with Easyfix hooks and holders
8 Mar, 2016

LogiMAT 2016: New GARANT ESD Workstation protects components against electrostatic discharges

 The Hoffmann Group presents its first ESD-proof GARANT Workstation at LogiMAT 2016 and demonstrates how EPA protection zones (Electrostatic Protection Area) should be set up in order to reliably shield sensitive components from electrostatic discharges. The new  GARANT Workstation for protecting against ESD (Electrostatic Discharge) is ESD powder-coated and conductive in accordance with DIN EN 61340-5-1. Electrostatic discharges are conducted from the work surface to a grounding cable on the underside of the worktop. This means that the workstation always remains charge-neutral. At LogiMAT 2016 the Hoffmann Group is located in hall 5, stand 5D55.

GO TO PRESS RELEASE

Messe-ESD-800x400.jpg
GARANT ESD Workstation