Press Releases
Full speed ahead – with GARANT Power Q
Milling with very high feed rates, without compromising process reliability – this is why the Hoffmann Group has now brought the new GARANT Power Q product family on to the market.

Hoffmann Group opens first subsidiary in the United States
The Hoffmann Group, Europe's leading system partner for quality tools, has officially opened its first subsidiary in the United States.

GARANT MasterSteel opens up a new performance class for solid carbide drills
The Hoffmann Group, Europe's leading system partner for quality tools, has expanded its GARANT MasterSteel product range with two new solid carbide drills, thereby further extending its lead over the competition when it comes to machining technology.

New platform for sharing information and expertise now on air
The Hoffmann Group has launched the Hoffmann Group TV online channel as an outlet for its film content. Through this new video portal, Europe's leading system partner for quality tools is now offering its customers a quick, convenient way of obtaining information on professional machining, milling, drilling, turning, measuring and grinding as well as state-of-the-art workstations and storage solutions – all from a single platform.

GARANT HB 7010-1 turning grade: the highest cutting speed for maximum productivity
The Hoffmann Group, Europe's leading system partner for quality tools, is introducing a new turning grade for steel machining to the market. The new GARANT HB 7010-1 turning grade was developed to achieve wear resistance at the highest cutting speeds.

LogiMAT 2016: GARANT access technology now with Easyfix hooks and holders
The Hoffmann Group is set to launch its new access technology products for the first time at LogiMAT 2016, in hall 5, stand 5D55. The new GARANT aluminium stepladders impress with added ergonomics and safety. This is ensured by the new Easyfix hooks and holders, which can be fitted simply to the side rails without the use of tools, making it easier and safer to carry electrical equipment and tools. This means that important equipment is always quickly to hand. As a result, working becomes more comfortable, more efficient and safer.

LogiMAT 2016: New GARANT ESD Workstation protects components against electrostatic discharges
The Hoffmann Group presents its first ESD-proof GARANT Workstation at LogiMAT 2016 and demonstrates how EPA protection zones (Electrostatic Protection Area) should be set up in order to reliably shield sensitive components from electrostatic discharges. The new GARANT Workstation for protecting against ESD (Electrostatic Discharge) is ESD powder-coated and conductive in accordance with DIN EN 61340-5-1. Electrostatic discharges are conducted from the work surface to a grounding cable on the underside of the worktop. This means that the workstation always remains charge-neutral. At LogiMAT 2016 the Hoffmann Group is located in hall 5, stand 5D55.