Extremely quick measuring, recording, managing, exporting or printing
1. Easy recording of the measurement points by tapping on the elements in the live display. Additional generation of measurement programme procedures with graphical working instructions for the following measurements.
2. Detailed graphical depiction of the measured elements in the view of the parts. This dimensioned drawing, together with the measurements record, can be printed out if required.
3. Elements view with tolerance input using various different calculation methods (Gauss, Pferch, Hüll, MMK, best form). Specified values can be input to the system by automatic rounding of the actual value, keyboard input or loading from a DXF file (using DXF option).
4. Comprehensive results lists with OK / Not OK displays and graphical tendency bars for deviations from tolerance. Measurement record with or without graphical depiction as printed output or data export (TSV/CSV/TXT).