Hoffmann Group Home
  • 500.000 listed articles
  • Delivery in 48h
  • TÜV certified quality of delivery
      • Meny
       

      Hearing protection – Preventing irreversible injuries

      7335_Gefahren_Kombination800px (1).jpg

      The illness is so vicious because is creeps up on you insidiously and is incurable. At first, affected people do not hear the higher tones. Only later is perception of the middle and lower tones impaired.
      This is particularly tragic because with the correct hearing protection every single case of noise-induced loss of hearing is 100% avoidable.

      Noise has a damaging effect not only on our hearing, it can generate damaging effects on the entire body. Noise stress can cause headaches, metabolic problems, digestive complaints and many other complaints.
      1 Headaches
      2 Tinnitus, hearing loss
      3 Increased risk of heart attack and high blood pressure
      4 Increase adrenaline flows with resulting metabolism issues
      5 Digestion problems
      6 Reduced blood flow

      At what point must hearing protection be worn?

      A noise is the result of vibrations propagated in the air as pressure waves. The more powerful the pressure waves the louder the noise. These can be measured and are stated in the unit decibel (dB). The stress of a noise level for the ear is stated in the unit dB(A).
      The protection of employees in a noisy working environment is regulated by the EC Noise Exposure Directive 2003/10/EC. This clearly specifies that at noise levels of 80 dB and above, hearing protection must be provided by the employer and that at noise levels 85 dB and above suitable hearing protection must be worn by the employee:
      No obligation to wear: ⌀ Noise level< 80 dB, noise pulses < 135 dB
      Supply but no obligation to wear: ⌀ Noise level 80 dB to 85 dB or noise pulses 135 dB to 137 dB
      Supply and obligation to wear: ⌀ Noise level > 85 dB, noise pulses > 137 dB
      The technical safety requirements specified in EN 352-1 to EN 352-8 must be satisfied.

      7335_Grenzwerte_3_1410px.jpg

      Select the right hearing protection

      The following points must be taken into account when choosing hearing protection:
      • Determine the noise level at the workplace.
      • Respect personal preferences, since these can have a decisive effect on wearer acceptance.
      • Note the SNR value for hearing protection products: This specifies how much the product reduces the prevailing noise levels.
      • If the frequency is known exactly, we recommend that the hearing protection is selected according to the H value (high frequency), M value (medium frequency) or L value (low frequency). Most industrial production processes generate predominantly medium frequency noise stress.
      • Do not choose noise insulation that is too high: below 70 dB residual noise level means too much protection, which leads to comprehension issues and feelings of isolation.
      • Residual noise level should be between 70 and 80 dB.

      7335_Laermpegel_2_1410px.jpg
      7335_Varianz_800px.jpg

      Variance: Depending on the type of hearing protection used, a correction value to allow for variance must be included: 5 dB for shell-type ear protectors; 5 dB for re-usable earplugs; 9 dB for disposable earplugs; and 5 dB for banded earplugs. The residual noise level can be determined as shown above.

      7335_Tragepausen_800px.jpg

      Important: Make sure that the hearing protection is worn 100% of the time in noisy working environments. Even short periods during which hearing protection is not worn lead to complete loss of the protective effect.

      Do you have any questions? Our experts are keen to help you at any time:

      To contact us about hearing protection advice

      Type of hearing protection

      Selection criteria for the right hearing protection

      7335_GehoerschutzStopsel_800px.jpg

      Disposable earplugs

      Earplugs are basically inserted into the auditory canal and are especially well-suited to moist and warm environments. They also have good attenuation levels due to filtration of the noise levels, even at low frequencies.

      7335_PlusMinus_1410px.jpg

      Advantages:
      • No perceptible weight, or only very small weight.
      • Can be combined with other protective equipment.
      • No heat build-up.
      • High availability from dispenser systems.

      In order to obtain the SNR values and hence optimum protection, correct insertion of the earplug is of critical importance.

      7335_Anleitung_Stoepsel_2_800px.jpg

      This is how to insert disposable earplugs correctly:
      1. Roll the plug up as small as possible, taking care not to fold it. Make sure your hands are clean.
      2. Reach over your head with your free hand and pull the ear upwards and backwards. Insert the plug deeply into the auditory canal.
      3. & 4. Hold the plug firmly for approx. 30–40 seconds until it has fully expanded within the auditory canal. The earplugs are seated correctly in the ear if nothing is visible when viewed from the front.

      This is the correct way to remove and dispose of earplugs:
      When removing the earplug, pull it slowly out of the auditory canal with a slight twisting action.
      After use, disposable earplugs should be disposed of in the correct manner.
       

      7335_wiederverwendbarerGehoerschutz_800px.jpg

      Re-usable earplugs

      Earplugs are basically inserted into the auditory canal and, due to the washable surface, they can be used again without losing their original shape. When you leave a noisy area, the earplugs can be put away in a handy storage box.

      7335_PlusMinus_1410px.jpg

      Advantages:
      • No perceptible weight, or only very small weight.
      • Can be combined with other protective equipment.
      • The cord means you won’t lose them.
      • Storage box for safe retention.

      Disadvantages:
      • Incorrect insertion reduces the attenuation performance.
      • Pressure sensation when worn for long periods.
      • Less suitable for fluctuating noise conditions.

      In order to obtain the SNR values and hence optimum protection, correct insertion of the earplug is of critical importance.

      7335_wiederverwendbarerGehoerschutz_Anleitung_2_800px.jpg

      This is how to wear earplugs correctly:
      1. Use one hand to grip the earplug by the stalk. With the other hand, pull the ear upwards and backwards whilst inserting the earplug into the auditory canal. Pulling the plug up and down during insertion increases the protective effect.
      2. Even when correctly seated, the plug remains visible from the outside.

      7335_wiederverwendbarerGehoerschutz_Box_800px.jpg

      Storage boxes:
      A small storage box, with a belt clip or kidney shape depending on the manufacturer, permits handy storage of earplugs when not in use. The cord means that the earplugs can be carried round the neck during breaks in work. Make sure your clothing is clean.

      7335_Buegelgehoerschutz_800px.jpg

      Banded earplugs

      Banded earplugs are easy to use, comfortable to wear and can be put on and taken off quickly. The earplug does not sit in the auditory canal, instead it closes off the outer opening of the canal, which makes it pleasant to wear. It is suitable for working environments with high temperatures, since no heat build-up occurs. Earplugs can be replaced and the band can be re-used.

      7335_PlusMinus_1410px.jpg

      Advantages:
      • Quick and easy positioning.
      • Pleasant to wear.
      • Low weight.

      In order to obtain the SNR values and hence optimum protection, correct insertion of the earplug is of critical importance.

      7335_Kapselehoerschutz_2_800px.jpg

      This is how to wear banded earplugs correctly:
      1. Grip the band under the chin with both hands.
      2. Pulling the ear upwards and downwards whilst inserting the earplug increases the attenuation rating.
      3. To check the seating, in a noisy environment press both earplugs slightly inwards. This should not make any great difference to the noise.

      This is how to exchange the earplugs on banded ear defenders:
      4. Pull the dirty earplug off the band.
      5. Insert the new earplugs on to the band with a slight twist.

      7335_Kapselehoerschutz_800px.jpg

      Shell-type ear defenders

      Shell-type ear defenders are particularly suitable for use in dirty environments and in environments where the noise level is continually changing. The capsule envelopes the entire ear, so the headband provides stable and comfortable seating. Nothing is inserted into the auditory canal. They are particularly suitable for persons whose auditory canals are very narrow and sensitive to pressure. Head straps, neck straps and chin straps are available with suitable mountings for use on safety helmets.

      7335_PlusMinus_1410px.jpg

      Advantages:
      • High attenuation rates can be achieved.
      • Easy to operate.
      • No sensation of pressure in the ear.
      • Easy to check if they are being worn.

      Disadvantages:
      • Sweating under the shell.
      • Higher weight.
      • Cannot always be combined with other protective equipment.

      In order to obtain the SNR values and hence optimum protection, correct insertion of the earplug is of critical importance.

      7335_Kapselehoerschutz_Anleitung_2_800px.jpg

      This is how to wear shell-type ear defenders correctly:
      1. Fold-away shell-type ear defenders from inwards to outwards.
      2. Place the shells over your ears.
      3. Adjust the position of the band upwards and downwards.

      The following should be taken into account during use:
      4. In order to avoid leakage, hair and the arms of glasses should not lie between the ear defender and the ear.
      5. The ears should no longer be visible.

      7335_Kapselehoerschutz_Helm_800px.jpg

      In combination with a safety helmet:
      1. The shell-type ear defenders can easily be put on or taken off by clicking on and off.
      2. When the ear defenders are not in use they can easily be swung away upwards.

      7335_Elektronischer_Gehoerschutz_800px (1).jpg

      Electronic hearing protection

      Hearing protection with special functions enables communication and simultaneous protection in the event of high noise levels. The noise-level-dependent attenuation technology means that warnings and instructions can audibly be received. Harmful noise is damped to a level less than 82 dB in order to protect hearing. Warning signals, discussions and process sounds are easily perceptible and communication over great distances in conjunction with mobile phones and radio devices is disruption-free. Additional functions, such as volume regulation of level-dependent functions, balance control, equalizer and volume control for external input signals, are available.

      7335_PlusMinus_1410px.jpg

      Advantages:
      • For demanding working environments.
      • Communication by radio or mobile phone.
      • Built-in conversational electronics fur use when work is monotonous.
      • Environmental noises are heard but noise pulses are automatically blocked off.
      • Increases in productivity and motivation of employees

      Disadvantages:
      • Unsuitable for occasional wearing.
      • Higher weight.
      • Heat build-up under the shell.

      In order to obtain the SNR values and hence optimum protection, correct insertion of the earplug is of critical importance.

      Diverse product range and personal consulting

      7335_Gehörschutz_Produktsortiment_800px.jpg

      At the Hoffmann Group, you will find a wide range of hearing protection products from selected and high-quality manufacturers for various fields of application: from the production hall to the construction site, right through to working in the forest or private use. We are able to supply high-quality earplugs and dispensers, banded earplugs, shell-type ear protectors, electronic hearing protection and matching accessories.

      Take advantage of our know-how in the field of PPE: We will provide you with professional support on all relevant issues from risk analysis, product choice, wearing tests right through to training your employees. Our highly qualified team of specialists will advise you personally on the subject of hearing protection. Get in touch with us, whether that be in person, by phone or via e-mail.

      Directives and standards for hearing protection

      7335_Paragraph_800px.jpg

      On 21 April 2018 the PPE regulation 2016/425 superseded the previous directive 86/686/EEC. This resulted in substantial changes to the classification of products in the field of personal protective equipment. As a result, the EU recognised that harmful noise causes irreversible harm to health and raised the classification of hearing protection products to risk category III. Special provisions are applicable to products in risk category III. Accordingly, in many EU member states, practical instruction by the company of the employees for category III protective equipment is a mandatory requirement. From 21 April 2019, manufacturers are only allowed to introduce to market hearing protection products in compliance with the new PPE regulation.

      The following European standards apply to hearing protection:
      EN 352-1: Shell-type ear defenders
      EN 352-2: Earplugs
      EN 352-3: Helmet ear defenders
      EN 352-4: Level-dependent shell-type ear defenders
      EN 352-5: Shell-type ear defenders with active noise compensation
      EN 352-6: Shell-type ear defenders with communication equipment
      EN 352-7: Level-dependent attenuating earplugs
      EN 352-8: Audio shell-type ear defenders for conversational applications (e.g. radio)
      EN 458: Recommendations for the selection, use, care and maintenance of hearing protection

      Frequently asked questions on hearing protection

      From which volume must hearing protection be worn?
      Hearing protection must be worn from a daily noise exposure level of 85 dB or a peak sound pressure level of 137 dB. According to the German Technical Regulations Governing Noise and Vibrations (TRLV), people with existing inner ear damage should consistently wear hearing protection from a daily noise exposure level of 80 dB and upwards.

      Up to which noise level can you wear earplugs?
      This depends on the type of SNR value (attenuating) of the earplug. Taking the correction value into account, an earplug with a high attenuation level can be used at higher noise levels than an earplug with a low attenuation level.

      Is the hearing protection used adequate for the activity?
      Selection programmes, which are available on a CD or on the Internet, are available for selecting the appropriate hearing protection.

      What does hearing protection do in terms of noise reduction?
      The level reduction can be 15–32 dB(A) for earplugs and 19–28 dB(A) for shell-type ear defenders.

      How were the limits determined?
      A panel of experts on “personal protective equipment” conducted an interlaboratory test with four analysis labs for certain constituent materials. In this process, different verification methods were also strategically employed. Suitable methods of analysis and quality criteria were defined based on the experiences from the interlaboratory tests. The levels of the individual limits were defined with the involvement of experts from the Institute for Occupational Safety and Health of the German Social Accident Insurance (BGIA) and taking account of the state of the art.

      Do you have any questions? Would you like to receive advice on PPE?

      Platzhalter_Beraterbild_4_800.jpg

      The Hoffmann Group provides you with everything from a single source:

      - We provide individual advice, tailored to your needs
      - Risk analysis, help with product selection, wearing tests, training sessions and special service offers (glove plans, skin protection plans) 

      Contact us now >