• Dear customers, due to maintenance work, there may be restrictions in the operation of the product navigation on 19.4. The search functions are available without restriction.

GARANT torque wrench

Electronic torque wrench with digital dial gauge display.

The next generation of torque wrench.

With the new electronic GARANT torque wrench with dial gauge display the Hoffmann Group is introducing the first dial gauge combined with digital display onto the market. Thanks to the TFT colour display taking a reading has become much more comfortable and reading errors are minimized. The GARANT torque wrench achieves an accuracy of ±2%.

The high-precision digital torque wrench , with a body of chrome-plated steel and an integral reversible ratchet with ejector, is ideal for controlled single tightening of screws and for control measurements.

Keeping an eye on precision

1. LED display

The green LED is illuminated: USB connection is established. Red LED is illuminated: The torque wrench is charging. Red LED is off: Charging is complete.

2. TFT colour display

Due to the combined digital and analogue display, reading errors are minimized in comparison to conventional dial gauges. The current torque (track) is displayed by the dial and a numeric value. After tightening, the peak value continues to be shown as an analogue and a digital display.

3. Battery charge level display

The remaining battery charge is shown on the battery charge display. To save power, the brightness of the screen is dimmed after approx. 30 seconds of inactivity. As soon as force is exerted the display returns to normal brightness. After approx. 2 minutes of inactivity the torque wrench switches off automatically.

4. Battery cover

The battery of the electronic torque wrench is easily changed.

5. Ergonomic handle with calibration point

Optimized handle design for optimum use of power and comfortable grip.

6. On / reset button

Intuitive operation via only one ON and Reset button.

7. Mini USB connection

The battery can be charged via this connection with the supplied mini USB cable.

8. Buzzer

An acoustic signal sounds as a warning shortly before the wrench's maximum torque is reached (overload protection).

9. Reversible ratchet with ejector

The pricing is also very appealing: Despite all the innovations the GARANT torque wrench with digital dial gauge is no more expensive than a conventional mechanical dial gauge with analogue display.

DIREKTKÖP

Logga in på ditt konto

I kundvagn

Till kundvagnen
Till kundvagnen