• Please note that the navigation structure for the Machining section has been revised. If you had filters set for the previous categories Mono-machining and Modular-machining, please check the newly set filters.
GARANT Multi Cut low-vibration burrs are available in ten different versions. They are available both uncoated and with a TiAlN coating.

GARANT multi-cut burrs: Low-vibration all-rounders for better surface finishes and higher metal removal rates

15 Jul 2021

With the new GARANT Multi Cut, the Hoffmann Group presents for the first time a new generation of general-purpose burrs. The low-vibration all-rounder burrs machine steel, stainless steel, aluminium and non-ferrous metals with high process reliability and are suitable for use both on manually-guided power tools and also in industrial robot cells. With their newly developed tooth geometry they generate about 30 percent less vibration than conventional burrs, and are particularly free-cutting. The results are plain to see: Better surface qualities, 50 percent longer tool life, 25 percent higher metal removal rate and up to 60 percent greater cutting performance.

The new burrs from the GARANT brand consist of an optimised carbide substrate and up to ten different profiles, coupled with the option of a TiAlN coating. The latter feature reduces heat input into the substrate, improves the chip evacuation and in addition increases the tool life.

With their innovative tooth pitch, the new GARANT Multi Cut burrs generate extremely low vibration values. That is particularly beneficial when used on manually-guided power tools, since the tool can be guided significantly more accurately, the surface quality is better and the operator experiences fewer physical effects due to vibration. All this with the most smooth cutting action, even at high depths of cut. In addition, the newly developed tooth geometry renders the burrs extremely free-cutting and ensures a high metal removal rate. Specially honed edges protect against premature wear and increase the tool life. The defined shaft surface quality prevents any slippage and provides secure clamping in the collet. The special qualities of the new GARANT Multi Cut burrs mean they are versatile across a wide range of applications.

The new GARANT Multi Cut burrs will be available from 1 August via the 2021/2022 Hoffmann Group catalogue, as well as in the eShop www.hoffmann-group.com.

To shopping cart