Hoffmann Group Home
  • 500.000 listed articles
  • Delivery in 48h
  • TÜV certified quality of delivery
      • Menu
      GARANT

      GARANT history:

      Today is tomorrow's yesterday.

      Nothing is more constant than change. 1973 marks the start and at the same time the origin of the GARANT brand in the area of machining. Since then, GARANT has made continual developments on your behalf so that, even the day after tomorrow, you will be at the head of the pack with the innovative premium quality from GARANT. The GARANT story – discover selected innovations and highlights:
      • garant1973.png

        1973

        GARANT Brand

        The GARANT brand is launched as the "clever alternative" in the field of machining.

      • garant1981.png

        1981

        Development start-up

        Start of development of the GARANT milling cutter range

      • garant1983.png

        1983

        GARANT milling cutter range

        The new GARANT milling cutter range is officially launched

      • garant1990.png

        1990

        End mill world premier

        Introduction of the world's first end mill as a 3-fluted version with 45° helix angles

      • garant1992.png

        1992

        GARANT Softcut

        Introduction of the new geometry for a reduction of cutting force

      • garant1994.png

        1994

        ISO 9001 certification

        We are the first sales company in this sector to be certified like a manufacturer

      • garant1998.png

        1998

        GARANT spanners and sockets

        Complete range of heavy-duty GARANT spanners and sockets launched onto the market

      • garant1999.jpg

        1999

        Research project

        GARANT achieves top results in the Kassel University research project "thread cutting in magnesium"

      • garant2001_1.png

        2001

        VDA 6.4 certification

        Further certification by the German Association of the Automotive Industry (VDA) underscores our manufacturer competence

      • garant2001_2.png

        2001

        GARANT machining handbook

        The first compendium of the industry, comprising more than 500 pages

      • garant2002.png

        2002

        GARANT colour coding system

        We are the first in the industry to introduce a system of colour coding for consistent machining of components

      • garant2003_1.jpg

        2003

        GARANT celebrates 30 years

        Release of the GARANT "anniversary box", containing a unique range of products, to mark
        the brand’s 30th year of existence

      • garant2003_2.png

        2003

        GARANT Diabolo

        The new type of coating developed especially for the hardest materials makes the GARANT Diabolo milling cutter range an immediate success

      • garant2004_1.png

        2004

        German market leadership

        With GARANT we become Germany's market leader in the field of solid carbide drilling and milling

      • garant2004_2.jpg

        2004

        Campaign

        The GARANT "animals" campaign is launched and receives numerous prizes and awards

      • garant2005.png

        2005

        GARANT powercard system launch

        The first "fully comprehensive insurance" for GARANT power tools, in a handy credit card format

      • garant2006.png

        2006

        GARANT MM1

        Introduction of the MM1 measuring microscope, a new HPC milling cutter range with ZOX coating, and the ToolCar

      • garant2007.png

        2007

        iF Award

        The GARANT torque wrench is recognised with the iF Award; in addition, the MTC milling cutter range is launched onto the market

      • garant2008.png

        2008

        GARANT Zeroclamp

        Introduction of the innovative zeropoint clamping system

      • garant2010_1.png

        2010

        GARANT 360°Tooling

        The premiere of the first all-round service for more productive machining processes

      • garant2010_2.png

        2010

        Modern materials

        Innovative cutting tools for new types of material open up new market segments for GARANT

      • garant2011.png

        2011

        GARANT ECO

        With "efficient cooling" GARANT sets new standards – just as with TopCut and the tooling range for lightweight components

      • garant2012Tieflochbohren.jpg

        2012

        GARANT deep hole drilling

      • garant2013HiPerDrill.jpg

        2013

        GARANT HiPer Drill