Hoffmann Group Home
  • 500.000 listed articles
  • Delivery in 48h
  • TÜV certified quality of delivery
      • Menu
      7482_PSA-Hautschutz_Header.jpg

      SKIN PROTECTION: IMPORTANT PREVENTATIVE MEASURES IN THE WORK PLACE

      FOUR-STEP APPROACH FOR OPTIMAL SKIN PROTECTION

      In the next section you will learn what the individual product categories encompass as well as what you should pay attention to when selecting products.

      Do you have any questions? Our experts are keen to help you at any time:

      To contact for skin protection advice>

      WHAT TO TAKE INTO CONSIDERATION WHEN SELECTING PRODUCTS

      So that your employees are optimally protected, skin protection starts even before work and is re-applied during work; these are preventative measures. Skin protection prevents work materials from penetrating into the skin and serves as a protective barrier against harmful substances. This makes it easier to clean the skin. Different skin protection products protect against things such as the following:

      ● Heavy soiling
      ● Strongly adhesive materials
      ● Water-based materials or wet environments
      ● UV radiation
      ● Moisture accumulation

      7482_Grafik_SanfteReinigung_800px.jpg

      Gentle skin cleansing

      Skin should be cleaned before, during and after work. Products from this category gently remove dirt without unnecessarily irritating the skin. Their effectiveness depends on the product; from light to medium soiling up to very heavy soiling, as well as strongly adhesive materials.   

      Hygienic hand disinfection

      In occupational areas in which hygiene plays and important role, hand disinfection is vital. It prevents the transfer of germs, bacteria as well as viruses and should take place before, during and after work.

      7482_Grafik_Feuchtigkeitsspende_800px.jpg

      Moisturising skin care

      In order to maintain the natural protective barrier of the skin, it requires lipids and moisture. In order to rejuvenate and soothe irritated skin, your employees can use appropriate skin care products after work. Depending on individual needs, there are products for normal, dry and irritated skin, as well as very dry and highly stressed skin. 

      Important ingredients in skin protection products

      Similar to many skin care products, specific active ingredients support skin moisturising, reduce itchiness and promote healing:

      Allantoin is a natural substance which promotes the healing of wounds and has cell-rejuvenating effects. It is used for alleviating skin irritations.  
      Glycerin prevents the loss of moisture in the skin. 
      Witch hazel is a plant extract from the hamamelidaceae family. It relieves slight itching and promotes the healing of wounds. 
      Panthenol is a provitamin. It strengthens the skin’s barrier function, increases the keratin layer’s ability to retain water, and improves the skin’s elasticity.  Additionally, it reduces inflammation and itching. 
      Emulsifiers are another important ingredient within skin protection. They help to combine liquids that do not mix, such as water and oil, into an emulsion.

      How to prevent product interactions and allergic reactions

      Ensure that the respective skin protectants are specifically suitable for each other in order to prevent interactions. This applies especially if you also use protective gloves as part of the personal protective equipment at your company. Some active ingredients in products may damage the material of the gloves.

      Healthy skin is essential in preventing allergies and intolerances which could result from certain substances in the work place. In order for the surface of the skin to remain intact, skincare plays an important role. Additionally, some products are free of ingredients such as silicones, parabens and soaps. 

      OCCUPATIONAL SKIN PROTECTION PLAN AS INSTRUCTIONS FOR YOUR EMPLOYEES

      7482_Grafik_Hautschutzplan_800x400px.jpg

      The skin protection and hygiene plan provides information on how you can optimally protect your skin. It also specifies which skin protectant is to be used in what scenario, and takes into account respective risks at the work place such as the work process. Our qualified team of experts in skin protection will advise you when creating this plan, as well as in selecting the appropriate products for your business.

      COMPREHENSIVE PRODUCT RANGE AND PERSONAL ADVICE

      7243_Hautreinigung_Produktsortiment_1410px.jpg

      Our expert team of PPE specialists will advise you at any time, so that you can protect your employees optimally. We support you in all respects when it comes to personal protective equipment, starting from risk assessments, product selection and wear tests, all the way to training your employees. In this regard, we are available for you in person, via e-mail or telephone. Additionally, we will advise you when creating the skin protection plan for your business: we will provide recommendations for treating the skin before work as well as for cleaning and care afterwards.

      FIRST AID AT THE WORK PLACE

      7482_Grafik_ersteHilfe.jpg

      Despite all precautionary and protective measures, employees may be injured while at work. In order to be able to help them quickly, first aid in the workplace is of utmost importance. 

      In this regard, first aid is required in the form of trained personnel who can step in during emergency situations, and provide appropriate assistance to the injured individual. The business must also ensure that appropriate aid material is available. This includes items such as:

      Dressing material
      First aid boxes and cabinets
      Eye washing

      Depending on type and size of the business as well as the occupational risks present, one or multiple first aid boxes with different contents may be required.

      Additionally, employers must fit signs within their business so that first aid facilities, storage locations for dressing material as well as first aid rooms can be located quickly. 

      FREQUENTLY ASKED QUESTIONS ABOUT SKIN PROTECTION

      What alternatives are there for employees who have an allergic reaction to a skin protection substance?

      People often have an allergic reaction to fragrances or preservatives. In this case, it is recommended that the person compare the substances listed in their allergy passport with the ingredients in the skin protectant. There are now also skin protectants which are declared free of perfume/fragrance/preservatives. 

      What is important when it comes to selecting skin protectants?

      Skin protectants should be harmless, appropriate for the task being performed and sufficiently effective. In addition to the manufacturer’s specifications, the company doctor should also be involved in the decision-making process.

      In which order should skin cleansers and skin disinfectants be used?

      To prevent skin irritations, the skin should be gently cleansed before disinfecting. Depending on the sector, the hygiene plan may also outline a different order of steps.  

      Do you have any questions? Would you like to receive advice on PPE?

      Platzhalter_Beraterbild_4_800.jpg

      The Hoffmann Group provides you with everything from a single source:

      - We provide individual advice, tailored to your needs
      - Risk analysis, help with product selection, wearing tests, training sessions and special service offers (glove plans, skin protection plans) 

      Contact us now >