Hoffmann Group Home
  • 500.000 vermelde artikelen
  • Levering binnen 24 h
  • TÜV-gecertificeerde leverkwaliteit
  • Menu

Nieuws

27-feb-2015

GARANT TopCut

Verkort uw insteltijden en verhoog uw productiviteit - snelle wissel en perfecte spanen. Versnel uw freesproces met de GARANT TopCut-assortimenten.

Presse_TopCut_400x289.jpg
GARANT TopCut
11-feb-2015

HOLEX ruwfrees ProSteel

Meer vermogen dan u zou verwachten. De nieuwe generatie HOLEX VHM-ruwfrezen: goede testresultaten bij de verspaning van staal. Profiteer ook van grote capaciteit voor een voordelige prijs.

Presse_ProSteel_400x289.jpg
Latest generation HOLEX solid carbide roughing end mill
14-jan-2015

Productinnovatie GARANT eco

GARANT 'efficient cooling' zet nieuwe standaards voor de draai- en steekbewerking. Voor meer flexibiliteit en efficiency - nu ook verkrijgbaar met de nieuwe GARANT eco VARIO-LINE.

Presse_ecoVarioLine_400x289.jpg
GARANT "efficient cooling"
30-sep-2014

Met de GARANT HiPer-Drill nieuwe toepassingsgebieden ontwikkelen

From 16th to 20th September 2014 the Hoffmann Group will be exhibiting in Hall 7, Stand A71 at the AMB International Exhibition in Stuttgart, where they will be presenting their latest innovations and products. One of the many highlights this year will be the latest development of the GARANT HiPer (High-Performance)-Drill. With an improved cooling system and new range of lengths, the range of flexible interchangeable head drills now opens up new fields of applications for customers.

HyperDrill5
The innovative cooling channels of the new GARANT HiPer-Drill ensure optimised cooling of the cutter inserts, together with very high process reliability.
16-sep-2014

Perfect surfaces when countersinking

With the GARANT 90° high-precision countersink 15 0305, the Hoffmann Group presents an innovative solution which avoids corrugated surfaces or lack of concentricity when countersinking. The extremely unequal spacing excludes the possibility of tool chatter. Not only does this achieve perfect surfaces, but the reduced loading ensures a longer tool life. The set of tools will be officially introduced at AMB in Stuttgart.

GARANT Kegelsenker 400.jpg
The special geometry of the GARANT 90° high-precision countersink guarantees perfectly smooth running and optimum results.
16-sep-2014

Precise clamping with the new GARANT high-pressure centring vice

With the new GARANT high-pressure centring vice, the Hoffmann Group presents at the AMB a product innovation for precise and reliable clamping. The product is characterised by being particularly easy to use and offering a wide variety of applications.

GARANT Zentrischspanner 400.jpg
The new GARANT high-pressure centring vice offers very high precision.