Gödde GmbH & Co. KG

Gödde GmbH & Co. KG was founded in 1960 in Cologne as Bert Gödde u. Söhne KG. The collaboration with Hoffmann started in 1973 and by 1993 it was only a small step to intensify the collaboration as a partner of the Hoffmann Group.

As a partner of the Hoffmann Group, Gödde is active in Germany, Belgium and Luxembourg.

 

 

Back | Top

On site in Cologne

v.l.n.r.: Max Wiemann, Jens Krakow, Oliver Gödde, Frederik Bauersch, Wilhelm Brühl
Der Stammsitz der Gödde GmbH & Co. KG in Köln.

Founded: 1960

Sales Director: Max Wiemann

Employees: 170

Partner of the Hoffmann Group since: 1993

Address:
Gödde GmbH & Co. KG
Robert-Perthel-Str. 57 – 59
50739 Köln
Germany

Phone: +49-2 21-59 90 6-0
Fax: +49-2 21-59 90 6-666

E-Mail: Kontakt
Website: www.goedde-werkzeuge.de

Back | Top